2022-10-17 03:48 AM
This only happens to new variables added to my C code after Oct 2022. "Old" variables still work fine. When I add failing variables to the "Expression" tab I get "Error: Multiple errors reported". Reported are:
Multiple errors reported.
1) Failed to execute MI command:
-var-create - * HelloWorld
Error message from debugger back end:
-var-create: unable to create variable object
2) Unable to create variable object
3) Failed to execute MI command:
-data-evaluate-expression HelloWorld
Error message from debugger back end:
No symbol "HelloWorld" in current context.
4) Failed to execute MI command:
-var-create - * HelloWorld
Error message from debugger back end:
-var-create: unable to create variable object
Does anyone have an idea? Looks like the debugger is not getting resources from Windows. I use 1.10.1 Build 12716_20220707_0928 (UTC)
Windows 11 Pro version 22H2
2022-10-19 02:19 AM
Hello @wvan .1
First let me thank you for posting.
Could you please provide the GDB client and server log, so I be able to further analyze the issue.
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-11-12 05:01 AM
i have similar problem: in debug / beakpoint no more variables shown at all ! shows declaration as if its in C editor mode. live expressions also no more working...just error msg.
see:
and blue -> detail:
is still same, when on OpenOCD instead of ST-LINK GDB-server.
problem maybe here:
or here, the root of all evil ?
and view expressions is now :
what can i do now , to get it working again ?
2022-11-13 01:53 AM
Java in linux system seem ok, all up to date.
$ java -version
openjdk version "1.8.0_332"
2022-11-15 02:49 AM
To analyze this further we need full log-files. Not only screenshots.
Is it even possible for you to share the projects with us? Would they be possible to run on an ST board? ... Hard to re-produce this issue!
What if you create a new debug configuration in the project with issues?
What if you create a new project, do you still have the same problem?
If same issue in a new project, then what if you change workspace?
Same problem? Re-installation of CubeIDE?
... Trying to go from a narrow scope to a wider scope to understand the issue.
Kind regards, Mattias
2022-11-15 07:46 AM
thx for your answer , Mattias .
-- even hard to describe all the "symptoms". 🙂
+
just some "impressions" from last days:
i installed older toolchain (gnu-tools-for-stm32.9-2020-q2-update), then working again.
i suppose, this actual problem is not to reproduce, because something happened in the IDE, similar a crash. I closed IDE , restart, looks ok. But was not really ok....
next i try to find some log files... and as test: make new project, as you recommend.
2022-11-15 10:25 AM
ok, big problem found : sitting at keyboard . :smirking_face:
for a speed test, i changed in a test project many optimizer and other setting, just also debug:
for some (idiot) reason, seems all projects got changed settings.... so turn to standard:
now variables shown in debug session again and start at "main" again.
other (small) problems with curious window switching in IDE still there.
need a beer now.
2022-11-15 11:32 AM
Dear Matthias, Ascha3,
Thanks for responding to my question on this forum. Un fortunately I am not able to share the code/project in which this problem occurred. I have however the following additional remarks:
I am not a proficient SDK specialist and do not know how to extract the GDB log files.
Friendly regards Willem