2023-11-21 07:29 AM
I use STM32CubeIDE on Linux Ubuntu (and to a lesser extent on MacOS and Windows, but I don't recall having a problem on the last 2 operating systems). About once or twice a day, at random, several of the keys such as <backspace> and <enter> and <delete> stop working. All the alphabetical and number keys work as normal. If I switch to a different application all the keys are working, but when I switch back to Cube the problem continues.
I solve the problem by saving my work, shutting and relaunching Cube. Is this a bug in the application?
Solved! Go to Solution.
2024-09-01 12:01 AM
Hi!
Are there any updates to this issue? As of 1 September 2024, this issue is still present on the Ubuntu operating system.
2024-09-05 04:16 AM
Hello,
I suggest that you download the last version of STM32CubeIDE through this link:
STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics.
In fact, this issue does not exist anymore on STM32CubeIDE 1.16.0 ; Ubuntu 22.04.
Thanks.
Mahmoud