cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to build two programs. Boot and app using STM32CubeIDE. For them use same make and linker files. They would need different *.ioc files

cgarland42
Associate III

MEMORY

{

 RAM    (xrw) : ORIGIN = 0x20000000,  LENGTH = 36K

 BOOT_FLASH (rx) : ORIGIN = 0x8000000,  LENGTH = 12K

 APP_FLASH (rx) : ORIGIN = 0x8003000,  LENGTH = 52K

}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
cgarland42
Associate III

I was able to have two build projects, and able to share common files etc..which is great.

But at the end I get:

Error: Cannot find the specified linker script. Check the linker settings in the build configuration.

make[1]: *** [makefile:91: fail-specified-linker-script-missing] Error 2

make[1]: *** Waiting for unfinished jobs....

make: *** [makefile:52: all] Error 2