2023-10-06 2:16 AM
I have a freshly installed stm32cubeide 1.13.2 on my ubuntu 22.04 machine and I've created a new workspace with a new project. In the beginning, everything works fine. But after generating code, closing the ioc file tab, closing the IDE and reopening the IDE with the same workspace and attempting to open the IOC file, it opens a blank tab failing to render the IOC file. If I close the tab and reopening it, the IDE hangs sometimes, or fails like before. It also seems to be using a whole lot of cpu resources. Reinstalling the IDE did not solve the problem.
2024-05-27 9:07 AM
It didn't in my case
2024-05-27 9:15 AM
I tried reinstalling the the IDE as well, as mentioned. But the problem clearly is not with the IDE, but with the related CubeMX software. So I'd call that the same symptoms as I had
2024-05-27 10:20 PM
Hi, I use CUBEMX on ubuntu 22.04 pretty much every day. I understand the problems encountered and at the beginning I also felt a certain amount of frustration. After several attempts I understood that there is certainly some problem but it could be mitigated. My development method was therefore to version the IOC file and proceed step by step.
When a blocking problem occurred I restored the previous version and started again. I've been working this way for almost a year now and I have to say it's working well.
Also keep in mind that the IO file can be opened with a file editor and is easy to understand.
Hope this is helpful.
2024-05-29 4:18 PM
My current work around is just to open the code and project in IDE but just the IOC file in CubeMX and it consistently works, albeit slowing down my workflow a bit.
2025-09-08 2:41 AM
You might use x11 rather than wayland (change on login screen).
Other option is to run the CubeMX with x11 backend on wayland:
GDK_BACKEND=x11 /opt/st/stm32cubeide_1.18.1/stm32cubeide
2025-11-02 7:07 AM
using GDK_BACKEND=x11 seems to solve the IOC rendering issue. But it very frequently causes the rest of the Eclipse UI to freeze, rendering it useless. Only thing that works is the menu and titlebar.