2026-04-21 8:58 AM
I have an old Ubuntu 18.04 system which allows STM32CubeIDE to run, but the STM32_Programmer failed because libm.so and libc.so were wrong. I found glibc-2.30 and copied the libraries into the same directory as the STM32_Programmer lib. Now I just get a seg fault, even when trying to just get the version number:
bin/STM32_Programmer_CLI --version
Segmentation fault (core dumped)Is there any way to figure out what might be the problem?
Solved! Go to Solution.
2026-04-29 1:50 AM
Hi @Mike Rosing,
Modern STM32CubeProgrammer releases (Post v2.16) have migrated to Qt6 instead of Qt5. This change introduced a compatibility break with older OS (Like Ubuntu 18.04).
What I suggest is to either update your OS or roll back to a previous tool version (v2.15 for example). Updating your OS is the better choice since you'll be able to utilize new STM32CubeProgrammer features and STM32s supported.
Hope you find this helpful !
Aziz
2026-04-21 11:09 AM
I found the crash dump, but I'm not able to make much sense of it:
#0 0x0000000000000000 in ?? ()
#1 0x00007fca818e4d58 in _dl_vdso_vsym (name=name@entry=0x7fca81936570 "__vdso_time",
vers=vers@entry=0x7ffdfb0c54b0) at ../sysdeps/unix/sysv/linux/dl-vdso.c:39
#2 0x00007fca8186c9b6 in time_ifunc () at ../sysdeps/unix/sysv/linux/x86/time.c:43
#3 0x00007fca83ba8d23 in elf_machine_lazy_rel (skip_ifunc=<optimized out>,
reloc=0x7fca817d9058, l_addr=140507732475904, map=0x7fca83d335e0)
at ../sysdeps/x86_64/dl-machine.h:577
#4 elf_dynamic_do_Rela (skip_ifunc=<optimized out>, lazy=<optimized out>,
nrelative=<optimized out>, relsize=<optimized out>, reladdr=<optimized out>,
map=0x7fca83d335e0) at do-rel.h:77
#5 _dl_relocate_object (scope=<optimized out>, reloc_mode=<optimized out>,
consider_profiling=<optimized out>, consider_profiling@entry=0) at dl-reloc.c:258
#6 0x00007fca83ba0327 in dl_main (phdr=<optimized out>, phnum=<optimized out>,
user_entry=<optimized out>, auxv=<optimized out>) at rtld.c:2190
#7 0x00007fca83bb6f50 in _dl_sysdep_start (start_argptr=start_argptr@entry=0x7ffdfb0c5900,
dl_main=dl_main@entry=0x7fca83b9e660 <dl_main>) at ../elf/dl-sysdep.c:253
#8 0x00007fca83b9e128 in _dl_start_final (arg=0x7ffdfb0c5900) at rtld.c:414
#9 _dl_start (arg=0x7ffdfb0c5900) at rtld.c:521
#10 0x00007fca83b9d098 in _start () from /lib64/ld-linux-x86-64.so.2
#11 0x0000000000000001 in ?? ()
#12 0x00007ffdfb0c5e62 in ?? ()
#13 0x0000000000000000 in ?? ()Maybe some other lib*.so needs to be updated as well?
2026-04-29 1:50 AM
Hi @Mike Rosing,
Modern STM32CubeProgrammer releases (Post v2.16) have migrated to Qt6 instead of Qt5. This change introduced a compatibility break with older OS (Like Ubuntu 18.04).
What I suggest is to either update your OS or roll back to a previous tool version (v2.15 for example). Updating your OS is the better choice since you'll be able to utilize new STM32CubeProgrammer features and STM32s supported.
Hope you find this helpful !
Aziz
2026-04-29 6:40 AM
Thank you for explaining the problem. To update the OS will break everything else, so I've decided to just get a whole new computer with the latest OS so I can use the STM32CubeProgrammer on the newer processors. The older OS will work fine as a network disk drive storage device so I don't lose all the previous projects.