2021-10-12 12:07 AM
I’m using cubeIDE and openOCD to debug on stm32f103. The interrupts not called although the interrupt flags are set. I tried to use GDB and they works fine for the same SW on the same board.
So how to make then working using openOCD?
I checked google and there are threads recommends using different startup code but I checked it and vector table seems to be ok and worked using GDB with the same startup code.
2021-10-12 8:51 PM
In order for an interrupt to fire:
Check those things.
2021-10-12 10:25 PM
All of them are ok. As I said the Interrupts are working when using GDB so no SW issue.
2021-10-13 6:51 AM