2024-03-18 11:22 PM
I have installed the example USB-C projects using the General/Import Projects from Folder or Archive option targeting the NUCELO-G474RE:
DRP1M1_DRP
SNK1M1_Sink
SNK1M1_Source
What do I need to do to make these regular STM32 projects such that the Build All, Build Project and Clean options are available (currently they are greyed out)?
Solved! Go to Solution.
2024-03-19 12:16 AM
Hello @alw and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to follow those steps:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-19 12:16 AM
Hello @alw and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to follow those steps:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-19 12:26 AM
Thanks very much, it all works ok now