cancel
Showing results for 
Search instead for 
Did you mean: 

Instabilities are occurring in Version 1.6.1

Not applicable

I'm using version 1.6.1 in linux, and there are several problems, for example, the main.c file opens but I can't use Delete or BackSpace keys, other times I can't edit the properties of the Device Configuration Tool. It has also occurred that the Device Configuration Tool cannot be opened completely, leaving a blank window within the Device Configuration Tool area.

To get around this, I quit the IDE and run it again.

These problems did not occur with version 1.5.

1 REPLY 1
Markus GIRDLAND
ST Employee

Hello there!

What version of Linux are you using?

I believe I can set up a test to try and reproduce this later today.