Instabilities are occurring in Version 1.6.1
Not applicable
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-13 3:33 PM
I'm using version 1.6.1 in linux, and there are several problems, for example, the main.c file opens but I can't use Delete or BackSpace keys, other times I can't edit the properties of the Device Configuration Tool. It has also occurred that the Device Configuration Tool cannot be opened completely, leaving a blank window within the Device Configuration Tool area.
To get around this, I quit the IDE and run it again.
These problems did not occur with version 1.5.
Labels:
- Labels:
-
STM32CubeIDE
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-21 1:27 AM
Hello there!
What version of Linux are you using?
I believe I can set up a test to try and reproduce this later today.