2024-05-14 6:06 AM
I want to use DMA with SPI in slave receive mode with words longer than 8 bits :
I launch the DMA with the function:
HAL_SPI_Receive_DMA( &HSPI_ADS, (uint8_t*)ads_dma_buffer, ADS_BUFFER_MAX_SIZE );
Unfortunately in this function the following test fails:
/* Packing mode management is enabled by the DMA settings */
if (((hspi->Init.DataSize > SPI_DATASIZE_16BIT) && (hspi->hdmarx->Init.DestDataWidth != DMA_DEST_DATAWIDTH_WORD) && \
(IS_SPI_FULL_INSTANCE(hspi->Instance))) || \
((hspi->Init.DataSize > SPI_DATASIZE_8BIT) && (hspi->hdmarx->Init.DestDataWidth == DMA_DEST_DATAWIDTH_BYTE)))
{
/* Restriction the DMA data received is not allowed in this mode */
errorcode = HAL_ERROR;
__HAL_UNLOCK(hspi);
return errorcode;
}
Because the structure "hspi->hdmarx->Init" is never initialized. It is not initialized, but the structure associated with the nodes is indeed initialized.
In the case where the data size is 8 bits, the test is correct because the returned and expected value is 0...
To validate the uninitialized "init" structure, I added the following code in the HAL_SPI_MspInit() function generated by the STMCubeMx
In my case it is SPI1 and the associated DMA is GPDMA1_Channel3. Obviously, the channel must be modified if another channel (or SPI) is used
__HAL_LINKDMA(spiHandle, hdmarx, handle_GPDMA1_Channel3);
if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel3, DMA_CHANNEL_NPRIV) != HAL_OK)
{
Error_Handler();
}
/* SPI1 interrupt Init */
HAL_NVIC_SetPriority(SPI1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI1_IRQn);
/* USER CODE BEGIN SPI1_MspInit 1 */
//-------------------------------------------------------------------------
#warning Ajout pour test correct dans MX_SPI1_Init() : verifier que ce soit le bon handle !
// Initialise le handle associé au DMA (idem hspi1.dmarx.Init après le link)
handle_GPDMA1_Channel3.Init = NodeConfig.Init;
//-------------------------------------------------------------------------
/* USER CODE END SPI1_MspInit 1 */
The problem here arises with the SPI, but it is a general initialization problem. This problem is hidden if the data size is 8 bits, because in this case the test in HAL_SPI_Receive_DMA() (or any similar function) becomes valid.
Solved! Go to Solution.
2024-05-22 7:44 AM
Hi @JVERN.18 ,
An internal ticket (ID: 181606) is submitted to the Development team to fix this issue.
Thank you for your contribution.
PS: Internal ticket (ID: 181606) is only for reference, not available outside of ST.
2024-05-15 2:21 PM
Hello @JVERN.18,
Thank you for having reported this.
Could you please share your ioc file which can be used to replicate the issue.
I will check the case and test with latest release of STM32CubeMX (v6.11.1) and STM32CubeU5 (v1.5).
2024-05-16 3:16 AM
2024-05-22 7:44 AM
Hi @JVERN.18 ,
An internal ticket (ID: 181606) is submitted to the Development team to fix this issue.
Thank you for your contribution.
PS: Internal ticket (ID: 181606) is only for reference, not available outside of ST.
2025-03-11 1:27 AM
Hi all,
Is there any update on the submitted ticket? I am having the same issue:
handle_GPDMA1_ChannelX.Init is not initialized
The NodeConfig structure is setup only locally inside MX_"QueueName"_Config function when I use generated linked_list.c file.
So in order for this hotfix to work:
handle_GPDMA1_Channel3.Init = NodeConfig.Init;
I need to copy pNodeConfig structure to get the Init settings from CubeMX.
Is there any other way how to initialize the Init structure for HAL_SPI_TransmitReceive_DMA to pass without errors?
Lukas
2026-01-21 1:48 PM
Is there any further information on this ticket?
It's now 2026 and I'm having that same issue with H5 and circular DMA (see my posting in CubeMX group).
2026-01-22 12:10 AM
Hello @Andrei Chichak ,
Sorry for the delay in resolving this issue.
I understand how this disruption has impacted your project, and that is not the experience we aim to provide.
I'm currently pushing to have this fixed in the next release, and I will update you as soon as it is resolved.
Thank you for your continued patience.
2026-01-22 12:16 PM
If at all possible, I'd settle for an interim work around so my colleague can continue testing.
2026-02-02 2:27 PM
Is there any estimated time frame on getting any sort of example code? We have an opportunity to redesign our circuit board to use an F4 instead of the H5 chip. Unfortunately it might be better to use a more mature processor.