2025-12-08 7:16 AM - last edited on 2025-12-08 7:36 AM by Andrew Neil
Why, oh why have you separated IDE and MX such that .ioc files can no longer be opened in IDE?
I cannot imagine any benefits and it makes the IDE significantly worse, such that I've felt compelled to revert to version 1.19.0 ( go to Help -> About STM32CubeIDE -> Installation Details -> Installation History -> select version -> Revert)
I couldn't find any other means of feeding back my strong dislike of this change other than a post like this. I hope version 2.1.0 comes out soon and re-integrates MX and IDE!
Solved! Go to Solution.
2025-12-12 1:37 AM
> These are all reasons against any IDE.
Yes, there are.
My company extensively uses CI now, and IDEs are only getting in the way of automated builds on remote servers. Especially if you want to support several architectures and thus several toolchains / IDEs.
We are using make files instead, which are easier to automate and deploy.
2025-12-12 12:54 PM - edited 2025-12-13 12:47 PM
We use Eclipse CDT as IDE and "headless" build tool for CI, for 20 years. Then we did this with Atollic, then with CubeIDE. As machines become faster, so does Eclipse :) But fashion is fashion. New generation obviously cannot like old stuff.
P.S. As for requests to run CubeMX code generation headless - I don't know. For long time I believed it is abuse of CubeMX and wrong idea generally. But now one could wish to use AI assistants with CubeMX as a "skill", in a fast try/test/modify loop... Hmm. From this POV decoupling CubeMX from the IDE looks even better :)
2025-12-23 8:11 AM
OK to sum things up: ST wants to cut costs. End of story.
2025-12-23 2:28 PM
Nothing to do with costs...
2026-01-01 3:05 PM
lets not hire more engineer to fix this
lets just remove it. Management at its peak!
2026-01-02 4:35 AM
It's not removed - it's just separated.
It doesn't seem unreasonable to do this so that the engineers can do actual useful stuff, rather than just deal with the added complications which integration brings - to little benefit..
2026-01-14 5:07 AM
There's a vote here in favour of the split !
2026-01-27 2:17 PM
Why, instead of improving and making the user's life easier, is the goal to make it more difficult,
susceptible to errors, and with senseless changes?
Besides the uncontable software bugs, an update every 3 months.
Give me a break.
2026-01-29 11:46 AM
Separation IDE and MX is bad idea.
Anyway, developer should have option to select integrated or separated tools.
Eclipse has good module structure and no problem to add addition plugins.
2026-01-29 11:56 AM
Strange opinion.
Eclipse has good module structure, no problem to install new bundles, remove or update selected bundles.
On developer workstation couple of gigabyte RAM not a problem. Start time is also not a problem. I start IDE not each week, simple send computer to sleep.