2020-01-27 9:08 AM
2020-01-27 9:20 AM
Error says what specifically? And what do those lines have on them? Most of this stuff can be troubleshooted if you provide sufficient/adequate information.
Some of the newer compilers have a lot more rigour in what they complain about, and aren't going to tolerate a redefinition of types.
Check the version of C/C++ the GNU compiler is implementing/enforcing, check if that is consistent with IAR
2020-01-27 9:34 AM
Usually, GCC does not just say "conflicting type" and leave it at that - it will usually go on to detail what type it was expecting, and what it saw instead.
As @Community member says, you haven't given enough detail to make any more specific suggestions.
You need to post the code that gives the error, and the complete, unabridged message - use copy & paste; do not manually re-type.
Use the 'Code Snippet' button.
2020-01-27 10:28 AM
I had a similar compiler issue because for gcc "int" is different type than "uint32_t" as return parameter of a function.
Maybe something like this ?
2020-01-29 5:07 AM
void parse_ipv6_address(uint8 *v, uint8 *buf)
{
uint8 value = 0;
uint8 offset = 0;
uint8 index = 0;
uint16 buffer_offset = 0;
uint8 temp_buff[10];
uint32 v6[4] = {'\0'};
temp_buff[0] = '\0';
uint8 i = 0;
//! Total 8 octets
for(index = 0; index < 8 ;index++)
{
//! each octet contains max of 5 characters including . dot
for(offset = 0;offset < 5 ; offset++)
{
value = buf[buffer_offset++];
if((value == '.') || (value == ':'))
{
break;
}
temp_buff[offset] = value;
}
temp_buff[offset]= '\0';
if(index % 2 == 0)
{
v6[index/2] = (parseHex(temp_buff) << 16);
}
else
{
v6[index/2] |= parseHex(temp_buff);
}
temp_buff[0] = '\0';
}
for(i = 0; i < 4; i++)
{
rsi_uint32_to_4bytes((v+(4*i)), v6[i]); // Function definition
}
}
the problem started when I migrated the code to gcc compiler.
void rsi_uint32_to_4bytes(uint8 *dBuf, uint32 val);
void rsi_uint16_to_2bytes(uint8 *dBuf, uint16 val);// function declaration
void string2array(uint8 *dst, uint8 *src, uint32 length);
../Core/Src/wifidrv/rsi_app_util.c:626:5: error: too many arguments to function 'rsi_uint32_to_4bytes'
the error is showing there is conflicting types and when i made changes it keep saying the above error.
2020-01-29 5:18 AM
for(i = 0; i < 4; i++)
{
rsi_uint32_to_4bytes((v+(4*i)), v6[i]); // Function definition
}
No, that is not the function definition!
That is a call to the function!
../Core/Src/wifidrv/rsi_app_util.c:626:5: error: too many arguments to function 'rsi_uint32_to_4bytes'
Note that this tells you exactly where the error is detected: it's at line 626 in the file rsi_app_util.c