2023-03-24 08:41 AM
i am using a STMCubeIDE v1.11.2 with windows 10 when i creat a new project it is working if i closed the IDE and open it again the problem below occure
Error in final launch sequence:
Failed to execute MI command:
target remote localhost:٦١٢٣٤
Error message from debugger back end:
localhost:?????: No such file or directory.
Failed to execute MI command:
target remote localhost:٦١٢٣٤
Error message from debugger back end:
localhost:?????: No such file or directory.
localhost:?????: No such file or directory.
this is a screenshot for the problem
2023-03-24 08:47 AM
Dupe https://community.st.com/s/question/0D53W00002CLJcoSAH/i-have-a-problem-on-debugging-nucleof446re
Not clear why your system display hieroglyphs instead of numbers.
Not sure how well any of this is tested on foreign language versions of windows.
2023-03-24 08:51 AM
this is number is 61234
2023-03-24 09:10 AM
I changed the number system of the windows from arabic to english and it is working now
2023-03-24 10:46 AM
Thanks for checking / confirming that.
@Imen DAHMEN @Amel NASRI @Sara BEN HADJ YAHYA
Can we push this into the respective teams to do some SW QA with different Windows Language / Locale settings. Thanks
2023-03-29 02:54 AM
Thanks @Community member for bringing this issue to our attention.
@Semer CHERNI will take care to investigate this issue.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.