cancel
Showing results for 
Search instead for 
Did you mean: 

I am trying to instal stm32 cube ide in my new Mac book air . there is error : This package is incompatible with this version of macOS. , . please help me for install cube ide in my new MacBook Air

Mrohi
Associate III

I am trying to instal stm32 cube ide in my new Mac book air . there is error : This package is incompatible with this version of macOS. ,The package is trying to install content to the system volume. Contact the software manufacturer for assistance.

. please help me for install cube ide in my new MacBook Air 

my Mac OS is Catalina

10.15

5 REPLIES 5
XThib.370
Associate

Same issue here with Catalina 10.15.1 Beta (19B77a). I have yet not managed to have it working but I slightly improved the situation:

I went to System Preferences > Security & Privacy > General and allowed STM32CubeIDE.app:

0690X00000Aql15QAB.png

IDE was able to launch but it takes a very long time with "Checking for Updated Files ..." modal. I cannot Cancel or Close this modal window.

As well, there is an issue with "st-stlink-server.1.2.0-3.pkg": This package is incompatible with this version of macOS.

0690X00000Aql3BQAR.png

​Installation log:

11:51:28+03 Installer[3042]: ST Link Server Installation Log

11:51:28+03 Installer[3042]: Opened from: /Volumes/STM32CubeIDE/st-stlink-server.1.2.0-3.pkg

11:51:28+03 Installer[3042]: No localized entry for ../common/license

11:51:28+03 Installer[3042]: Package Authoring Error: <background_scaling> has an unsupported MIME type: X-NSObject/NSNumber

11:51:28+03 Installer[3042]: Package Authoring Error: <background_alignment> has an unsupported MIME type: X-NSObject/NSNumber

11:51:28+03 Installer[3042]: Package Authoring Error: <layout-direction> has an unsupported MIME type: X-NSObject/NSNumber

11:51:28+03 Installer[3042]: Failed to load specified background image

11:51:28+03 Installer[3042]: Product archive /Volumes/STM32CubeIDE/st-stlink-server.1.2.0-3.pkg trustLevel=100

11:51:28+03 Installer[3042]: External component packages (1) trustLevel=100 (trust evaluation failed: Error Domain=PKInstallErrorDomain Code=101 "The package “st-stlink-server.1.2.0-3.pkg�? is not signed." UserInfo={NSURL=#tmp.pkg -- file:///Volumes/STM32CubeIDE/st-stlink-server.1.2.0-3.pkg#Distribution, PKInstallPackageIdentifier=com.st.pkg.st-stlink-server, NSLocalizedDescription=The package “st-stlink-server.1.2.0-3.pkg�? is not signed.})

11:51:28+03 Installer[3042]: Could not load resource readme: (null)

11:51:28+03 Installer[3042]: No localized entry for ../common/license

11:51:28+03 Installer[3042]: Could not load resource license: (null)

11:51:57+03 Installer[3042]: ================================================================================

11:51:57+03 Installer[3042]: User picked Standard Install

11:51:57+03 Installer[3042]: Choices selected for installation:

11:51:57+03 Installer[3042]: Install: "ST Link Server"

11:51:57+03 Installer[3042]: Install: "Install"

11:51:57+03 Installer[3042]: st-stlink-server.1.2.0-3.pkg#tmp.pkg : com.st.pkg.st-stlink-server : 1.2.0-3

11:51:57+03 Installer[3042]: ================================================================================

11:51:57+03 Installer[3042]: It took 0.00 seconds to summarize the package selections.

11:51:57+03 Installer[3042]: -[IFDInstallController(Private) _buildInstallPlanReturningError:]: location = file://localhost

11:51:57+03 Installer[3042]: -[IFDInstallController(Private) _buildInstallPlanReturningError:]: file://localhost/Volumes/STM32CubeIDE/st-stlink-server.1.2.0-3.pkg#tmp.pkg

11:51:57+03 Installer[3042]: Set authorization level to root for session

11:52:08+03 Installer[3042]: Administrator authorization granted.

11:52:08+03 Installer[3042]: Will use PK session

11:52:08+03 Installer[3042]: Using authorization level of root for IFPKInstallElement

11:52:08+03 Installer[3042]: Package Authoring Error: Package contains system volume install location content. Installation cannot proceed since installing to the system volume is not possible.

11:52:08+03 Installer[3042]: Package Authoring Error: Package contains system volume install location content, and installation will fail: Error Domain=IFInstallErrorDomain Code=-6000 "This package is incompatible with this version of macOS." UserInfo={NSLocalizedRecoveryOptions=(

  Quit

), IFReadOnlyPathsKey={(

  "/delivery"

)}, NSLocalizedRecoverySuggestion=The package is trying to install content to the system volume. Contact the software manufacturer for assistance., NSLocalizedDescription=This package is incompatible with this version of macOS.}

11:52:14+03 Installer[3042]: Client requested cancelation of install following warning.

11:52:14+03 Installer[3042]: Halting PK session due to client response to warning This package is incompatible with this version of macOS.

11:52:14+03 Installer[3042]: Install failed: The Installer could not install the software because there was no software found to install.

Mrohi
Associate III

I have solve other way . 1 first from Catalina downgrade to Mojave and then install old version cube ide and update all cube ide then upgrade to Catalina . and working very nice happily .:grinning_face: .

Mrohi
Associate III

0690X00000ArJxDQAV.png

RichardS1
Associate II

How can we push this bug into STM32 stlink driver developers?

ecode
Associate II

The problem continues.