2019-12-26 4:39 AM
macOS high Sierra
version 10.13.6
I am unable to access log file under /tmp
I can program this board from a pc
Full console report:
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_ORi32V.log
ST-LINK SN : 0672FF575251717867142819
ST-LINK FW : V2J35M26
Voltage : 3.21V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Cannot identify the device
Error: unknown or unsupported device (DevID = 0x0000)
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_kyXyTR.srec
File : ST-LINK_GDB_server_kyXyTR.srec
Size : 38932 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.278
Verifying ...
Error: Data mismatch found at address 0x08000004 (byte = 0xCD instead of 0x09)
Error: Download verification failed
2019-12-26 5:29 AM
Change GDB server to OCD and try again, if not try under reset. All in debug configuration .
Most errors I see here is when using macOs =) Did You tried it on normal liniux?
Looks like You download software correctly, but in config of mcu you diasable swd, so st link cant find target 0x0000 and cant verify.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.