2023-05-01 11:00 AM
Open On-Chip Debugger 0.12.0-00017-gb153daa14 (2023-02-03-14:58)
Licensed under GNU GPL v2
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J41S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.240714
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x0bb11477
Info : [STM32F030F4Px.cpu] Cortex-M0 r0p0 processor detected
Info : [STM32F030F4Px.cpu] target has 4 breakpoints, 2 watchpoints
Info : starting gdb server for STM32F030F4Px.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : device id = 0x10006444
Info : flash size = 32 KiB
Warn : GDB connection 1 on target STM32F030F4Px.cpu not halted
undefined debug reason 8 - target needs reset
shutdown command invoked
Info : dropped 'gdb' connection
2023-05-05 7:20 AM
Hi @DHirs.2
The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.
Regards,
Billy
2024-05-07 12:54 PM
Unfortunately I have same problem. Is there any news about this problem??
Open On-Chip Debugger 0.12.0-00029-gf77e7cb03 (2023-12-15-13:25) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J45S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.231196
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x0bb11477
Info : [STM32F030F4Px.cpu] Cortex-M0 r0p0 processor detected
Info : [STM32F030F4Px.cpu] target has 4 breakpoints, 2 watchpoints
Info : starting gdb server for STM32F030F4Px.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : device id = 0x10006444
Info : flash size = 32 KiB
Warn : GDB connection 1 on target STM32F030F4Px.cpu not halted
undefined debug reason 8 - target needs reset
shutdown command invoked
Info : dropped 'gdb' connection
2024-05-07 1:25 PM
ST is not going support boot-leg or counterfeit equipment.
Did it even program this part?
You should check if you can connect use STM32 Cube Programmer independently.
You need VCC, SWDIO, SWCLK, NRST and GND wired to the programmer.
On low pin count devices make sure your code doesn't break debugger connectivity by disabling or reassigning pins.
If you have a BOOT0 pin, pull it HIGH to stop your code running