2023-07-26 04:47 PM
Hi,
In STM32CubeIDE 1.12.1 I right-clicked on a .c file in the Project Explorer view and excluded it from build. Now I want to include it back in my build. How do I do that from the IDE?
thanks,
russ
Solved! Go to Solution.
2023-07-26 05:25 PM
Go to the "Exclude from build" dialog again, uncheck the boxes for Debug and Release and hit OK to include the file back into the build.
2023-07-26 05:25 PM
Go to the "Exclude from build" dialog again, uncheck the boxes for Debug and Release and hit OK to include the file back into the build.
2023-07-26 06:34 PM
The file I excluded disappeared from the Project Explorer window. When I excluded it I right-clicked on it then Resource Configurations->Exclude from build. How do I get back to the "Exclude from build" window for a file that is missing from the Project Explorer window?
thank you
2023-07-26 06:35 PM
Wow, never mind. I see it greyed out at the bottom of the Project Explorer window. Sorry I wasted your time. :|
2024-09-05 01:35 AM
Answer to this question totally depends on what kind of file you want to undo " exclude the build ".
1) for header files (xxx.h) --> go to header file, left-click and select properties (Alt + enter), navigate to resource section, select C/C++ build tab. click on configuration tab and select [all configurations]. Uncheck the box Exclude resource from build. Apply and Close.
2) for source files (xxx.c) --> left click on .c file and click Resource Configuration and select Reset to Default.
I hope that helps for you,
Thanks😀