How to obtain the dwarf2 file to simulate with proteus isis
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-01 2:05 PM
Hi all, I'm trying to simulate a project made in STM32Cube IDE for an STM32F103C6 in proteus ISIS but for debug purposes labcenter's people says that I need the .elf file and the dwarf2 file (both of them in the same folder), then I' found that GCC for STM32Cube IDE generates the dwarf 2 file with the option -gdwarf-2 what I've put in Project Properties -> Build steps and in the pre-build command I've wrote the command -gdwarf-2, it didn't worked so I've changed the command to the post-build commands in the same tab. I've also noted that in Tool Settings are several options for what I think is to choose the type of dwarf file that is going to be made during compilation but the only options are none, minimal (-g1), default (g) and maximum (-g3).
After I did this the output of the compilations shows the following message:
20:27:10 **** Incremental Build of configuration Debug for project Cubex ****
make -j4 all
gdwarf-2
make (e=3): El sistema no puede encontrar la ruta especificada.
make[1]: [makefile:81: pre-build] Error 3 (ignored)
arm-none-eabi-size Cubex.elf
text data bss dec hex filename
16752 20 1796 18568 4888 Cubex.elf
Finished building: default.size.stdout
20:27:28 Build Finished. 0 errors, 0 warnings. (took 17s.509ms)
I think this means that it couldn't make the dwarf2 file due the message "El sistema no puede encontrar la ruta especificada" (The system can not find the specified path).
Can anyone help me and explain how to obtain the needed files. Thanks in advance for the help.
- Labels:
-
STM32CubeIDE
-
STM32F1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-01 2:38 PM
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
‎2020-07-01 2:41 PM
Sorry, I was thinking that it was another kind of forum.