2020-07-01 6:16 PM
I'm having an issue where STM32CubeIDE is experiencing a Java exception when I attempt to create a STM32 Project.
The following is the output from the IDE log
!SESSION 2020-07-01 17:40:06.274 -----------------------------------------------
eclipse.buildId=Version 1.3.1
java.version=1.8.0_202
java.vendor=AdoptOpenJdk
BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_US
Command-line arguments: -os win32 -ws win32 -arch x86_64 -data C:\Users\jomodev\STM32CubeIDE\workspace_1mems
!ENTRY com.st.stm32cube.ide.mcu.informationcenter 1 1 2020-07-01 17:40:15.371
!MESSAGE Log4j initialized with config file C:\Users\jomodev\STM32CubeIDE\workspace_1mems\.metadata\.log4j.xml
!ENTRY com.st.stm32cube.ide.mcu.ide 1 1 2020-07-01 17:40:19.969
!MESSAGE Started RMI Server, listening on port 41337
!ENTRY com.st.stm32cube.ide.mcu.ide 4 4 2020-07-01 17:40:20.994
!MESSAGE com.st.stm32cube.ide.mcu.ide/META-INF/version/build_ref file not found, build reference will not be reported into properties
!SESSION 2020-07-01 18:01:25.398 -----------------------------------------------
eclipse.buildId=Version 1.3.1
java.version=1.8.0_202
java.vendor=AdoptOpenJdk
BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_US
Command-line arguments: -os win32 -ws win32 -arch x86_64
!ENTRY com.st.stm32cube.ide.mcu.informationcenter 1 1 2020-07-01 18:04:01.045
!MESSAGE Log4j initialized with config file C:\Users\jomodev\STM32CubeIDE\workspace_1mems\.metadata\.log4j.xml
!ENTRY com.st.stm32cube.ide.mcu.ide 1 1 2020-07-01 18:04:07.595
!MESSAGE Started RMI Server, listening on port 41337
!ENTRY com.st.stm32cube.ide.mcu.ide 4 4 2020-07-01 18:04:08.438
!MESSAGE com.st.stm32cube.ide.mcu.ide/META-INF/version/build_ref file not found, build reference will not be reported into properties
!ENTRY org.eclipse.ui 4 0 2020-07-01 18:04:27.703
!MESSAGE Unhandled event loop exception
!STACK 0
java.lang.NullPointerException
at com.st.stm32cube.common.ecosystemintegration.ui.core.MCUEcoSystemIntegrationUiHelper.getTargetSelector(MCUEcoSystemIntegrationUiHelper.java:78)
at com.st.stm32cube.common.projectcreation.ui.wizard.TargetSetupPage.createControl(TargetSetupPage.java:92)
at org.eclipse.jface.wizard.Wizard.createPageControls(Wizard.java:179)
at org.eclipse.jface.wizard.WizardDialog.createPageControls(WizardDialog.java:743)
at org.eclipse.jface.wizard.WizardDialog.createContents(WizardDialog.java:635)
at org.eclipse.jface.window.Window.create(Window.java:431)
at org.eclipse.jface.dialogs.Dialog.create(Dialog.java:1094)
at org.eclipse.ui.internal.actions.NewWizardShortcutAction.run(NewWizardShortcutAction.java:119)
at org.eclipse.jface.action.Action.runWithEvent(Action.java:474)
at org.eclipse.jface.action.ActionContributionItem.handleWidgetSelection(ActionContributionItem.java:580)
at org.eclipse.jface.action.ActionContributionItem.lambda$4(ActionContributionItem.java:412)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:4173)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1057)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:3986)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3585)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1160)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1049)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:633)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:557)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:150)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:150)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:137)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:107)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:400)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:660)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:597)
at org.eclipse.equinox.launcher.Main.run(Main.java:1468)
!ENTRY org.eclipse.ui 4 4 2020-07-01 18:04:59.647
!MESSAGE Failed to retrieve data for section: section.installed.bundles
!STACK 0
java.lang.NullPointerException
at java.util.HashMap.merge(HashMap.java:1225)
at java.util.stream.Collectors.lambda$toMap$58(Collectors.java:1320)
at java.util.stream.ReduceOps$3ReducingSink.accept(ReduceOps.java:169)
at java.util.Spliterators$ArraySpliterator.forEachRemaining(Spliterators.java:948)
at java.util.stream.AbstractPipeline.copyInto(AbstractPipeline.java:481)
at java.util.stream.AbstractPipeline.wrapAndCopyInto(AbstractPipeline.java:471)
at java.util.stream.ReduceOps$ReduceOp.evaluateSequential(ReduceOps.java:708)
at java.util.stream.AbstractPipeline.evaluate(AbstractPipeline.java:234)
at java.util.stream.ReferencePipeline.collect(ReferencePipeline.java:499)
at org.eclipse.e4.core.internal.services.about.InstalledBundles.append(InstalledBundles.java:36)
at org.eclipse.ui.internal.about.ConfigurationLogDefaultSection.appendSection(ConfigurationLogDefaultSection.java:65)
at org.eclipse.ui.internal.about.ConfigurationLogDefaultSection.write(ConfigurationLogDefaultSection.java:49)
at org.eclipse.ui.internal.ConfigurationInfo.appendExtensions(ConfigurationInfo.java:102)
at org.eclipse.ui.internal.ConfigurationInfo.getSystemSummary(ConfigurationInfo.java:74)
at org.eclipse.ui.internal.about.AboutSystemPage.lambda$0(AboutSystemPage.java:142)
at org.eclipse.core.runtime.jobs.Job$1.run(Job.java:164)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
2020-07-01 7:29 PM
STM32CubeIDE doesn't play well with OpenJDK. This question has come up before. Some people have found workarounds:
2020-07-01 7:49 PM
Interesting. I have no indication that I have OpenJDK install on the system so I am not sure where it is picking this up from.
java -version
java version "1.8.0_251"
Java(TM) SE Runtime Environment (build 1.8.0_251-b08)
Java HotSpot(TM) 64-Bit Server VM (build 25.251-b08, mixed mode)
2020-07-02 3:02 AM
Weird. I just assumed since your log shows "java.vendor=AdoptOpenJdk".
In any case, the log doesn't match what you're getting back with the "java -version" command. The version number is different as well. Likely there is another Java version floating around somewhere.
2020-07-02 8:19 AM
Looks like STM32CubeIDE install this AdoptOpenJDK version of Java:
H:\Development\STM\STMicroelectronics\STM32CubeIDE_1.2.0\STM32CubeIDE>jre\bin\java -version
openjdk version "1.8.0_202"
OpenJDK Runtime Environment (AdoptOpenJDK)(build 1.8.0_202-b08)
OpenJDK 64-Bit Server VM (AdoptOpenJDK)(build 25.202-b08, mixed mode)So, if STM32CubeIDE does not play well with OpenJDK, then why did it install this version of Java?
2020-07-02 8:34 AM
2020-07-02 8:41 AM
Actually, your comments were helpful in narrowing it down to where the extra Java version was and I appreciate your responses.
Now to understand why it will not work in my env. Perhaps since I have the tool installed in an non "c:\" location is is causing a path issue.
I'll have to play with this and see if I can resolve it. I do have a version that is working on a Ubuntu VM which will work in the mean time.
Cheers,
Jon
2020-07-02 12:13 PM
So, I removed the 1.3.1 version of STM32CubeIDE and then installed the 1.3.0 version and now it is working again. Interesting, this version also uses OpenJDK but a newer version.
C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE>jre\bin\java.exe -version
openjdk version "1.8.0_242"
OpenJDK Runtime Environment (AdoptOpenJDK)(build 1.8.0_242-b08)
OpenJDK 64-Bit Server VM (AdoptOpenJDK)(build 25.242-b08, mixed mode)One note though, I did let it install into the default location of "C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE"
I'll just ignore the update to 1.3.1 for the time being.