2019-09-03 3:30 PM
st-stm32cubeide_1.0.2_3566_20190716-0927_x86_64.exe
is supposed to install the toolchain. But it is a 64 bit application that cannot be started on a 32 bit Windows system
2019-09-03 4:10 PM
Step 1: Upgrade Windows to 64-bit.
Step 2: install the CubeIDE
-- pa
2019-09-03 5:25 PM
One more reason of why Eclipse is not a normal IDE...
2019-09-04 12:47 AM
I have used Windows 64bit for several years, and am experiencing lack of performance on the machine with 4GB.
So I have decided to step back to the x86 version, and have other packages that will only run on 32 bit systems.
Dual boot maybe an option, but the description suggests that st-stm32cubeide is designed to run on either OS.