cancel
Showing results for 
Search instead for 
Did you mean: 

How to install the toolchain on a computer with 32bit Windows 10 … ?

st-stm32cubeide_1.0.2_3566_20190716-0927_x86_64.exe

is supposed to install the toolchain. But it is a 64 bit application that cannot be started on a 32 bit Windows system

3 REPLIES 3
Pavel A.
Evangelist III

Step 1: Upgrade Windows to 64-bit.

Step 2: install the CubeIDE

-- pa

Piranha
Chief II

I have used Windows 64bit for several years, and am experiencing lack of performance on the machine with 4GB.

So I have decided to step back to the x86 version, and have other packages that will only run on 32 bit systems.

Dual boot maybe an option, but the description suggests that st-stm32cubeide is designed to run on either OS.