2022-04-07 05:33 PM
Where can I download an archive of the GNU Tools for STM32 separate from the STM32Cube IDE?
Alternatively where can I find your open-sourced patches that you list in the information center?
2023-09-06 06:58 AM
@jemason That is exactly what I want to do - create docker images with different versions of the toolchain. It would be great to be able to to that without having to install the whole IDE.
I would consider seperating the build system/process from the IDE good practice. Shouldn't that alone be a good reason for ST to provide the toolchaine binaries as separate downloads?
2023-10-03 01:07 AM
We are also looking for a way of creating a Docker image with the build tools for CI/CD without the whole IDE. Any news on this?
2023-10-03 04:46 AM
Are there any reason why don't use the official precompiled GNU toolchains binaries from ARM?
ARM GNU Toolchains for R/M-Profile (binutils, gcc, newlib) ONLY*:
https://developer.arm.com/downloads/-/gnu-rm
*) Toolchains only, no STM32 libraries like HAL
2023-10-03 06:02 AM - edited 2023-10-03 06:03 AM
2023-12-10 02:50 AM
ST apply patches to the tool chain - so the official one is not the same as the ST one.
2023-12-13 02:38 AM
Hello,
To get more visibility and investigate your issue, could you post the question in a new community thread?
Thanks,
Rim
2024-03-08 12:38 AM
Any news on this or where can I find the new community thread?