2024-12-16 05:02 AM
Hello,
I recover from a project but when I compile there are errors.
And yet this file exists in the project
I think that in this tab the configuration is not correct, how can I change the configuration so that it is taken into account in my workspace ?
Thank you for your helps.
Regards
2024-12-16 05:11 AM
@DYann.1 wrote:I recover from a project
What do you mean by that?
@DYann.1 wrote:
Thank you for your helps.
Regards
That path has a leading slash - you probably don't want that.
The easiest way to ensure that a folder is correctly included in the Include Paths is to right-click that folder, and choose 'Add/remove include path...'
2024-12-16 05:19 AM - edited 2024-12-16 05:20 AM
@Andrew Neil wrote:
@DYann.1 wrote:I recover from a project
What do you mean by that?
@DYann.1 wrote:
When compiling there are errors, and the file is configured like this, I haven't modified anything
@Andrew Neil wrote:The easiest way to ensure that a folder is correctly included in the Include Paths is to right-click that folder, and choose 'Add/remove include path...'
I'll try this option to see.
2024-12-16 05:47 AM
I don't have the same version
I'll update the STM32CubeIDE version
2024-12-16 06:23 AM
I'm looking at how to correctly install STM32CubeIDE updates, in fact last time I lost all my programs. Caution !
2024-12-17 01:26 AM - edited 2024-12-17 01:29 AM
@DYann.1 wrote:I don't have the same version!
What version do you have?
The screenshot is from v1.13.0 - so it's not a very recent addition
@DYann.1 wrote:I'm looking at how to correctly install STM32CubeIDE updates, in fact last time I lost all my programs.
You already have a separate thread on that:
https://community.st.com/t5/stm32cubeide-mcus/update-stm32cubeide/td-p/754230
As noted there, updating should not lose all your projects!