cancel
Showing results for 
Search instead for 
Did you mean: 

How to associate .cproject and .project files to STM32CubeIDE in Mac OS?

dibor
Associate

Hello.

Cube IDE has option in the settings to associate .cproject and .project files to STM32CubeIDE.

dibor_0-1737486219616.png

But nothing changed in the project folder :(

dibor_1-1737486320805.png

I have tried to give "full disk access" to the STM32CubeIDE application - but nothing change.
STM32CubeIDE application has ProjectImporter.app into the application package, but I do not know how to use it :(

If I try to do "open with" STM32CubeIDE -  .cproject file opens as xml file in STM32CubeIDE :(

How can I import project?

 

Thank U

3 REPLIES 3
Pavel A.
Evangelist III

It is best to NOT associate .project and .cproject files with CubeIDE, on any OS. Because these files can be Eclipse projects of any nature, STM32 or not. Also, consider that several CubeIDE versions are installed on one host. Which one should run? For this reason these files are "hidden". 

So how do you open these projects? Simple. Start the needed version of CubeIDE (or other Eclipse) and open the needed workspace. Then import the project into that workspace. Next time when you start the CubeIDE you can specify the default workspace to open automatically.

One could wish that opening .project files from OS shell would start some "version selector" like in MS Visual Studio, but someone should make that tool, and IMHO it's not worth it.

STM32CubeIDE application has ProjectImporter.app into the application package, but I do not know how to use it :(

Then, welcome to the User Guide )) As the ancient saying goes... if nothing helps - read the documentation ))


@Pavel A. wrote:

Then import the project into that workspace.


Hi.

Which import option to choose?

dibor_0-1737525041772.png

Without RTFM impossible to import ?

 

amjad374
Visitor

Try manually opening the project from STM32CubeIDE using "File > Open Project" and select the folder containing your .cproject and .project files. If that doesn't work, you can try resetting STM32CubeIDE's preferences by going to ~/Library/Preferences and deleting the IDE settings, then reattempt the import.