2021-03-28 9:54 AM
I created the project initially using CubeMX using a 128k STM32G431. I've ended up actually using a 64k ram part instead. The CubeIDE project calls out the wrong part now.
Because of extensive changes in the source code I do NOT want to re-run CubeMX with the new part. I'd like to manually change the necessary files so CubeIDE reports a 64k ram part.
Thanks,
Brian
Solved! Go to Solution.
2021-03-28 10:27 AM
If only the RAM is bothering you, you can simply compare the .ld files for both chips and copy over the correct lines. A cleaner way is described here: https://community.st.com/s/question/0D53W00000cyiAcSAI/porting-project-to-pin-compatible-mcu-in-stm32cubeide
2021-03-28 10:27 AM
If only the RAM is bothering you, you can simply compare the .ld files for both chips and copy over the correct lines. A cleaner way is described here: https://community.st.com/s/question/0D53W00000cyiAcSAI/porting-project-to-pin-compatible-mcu-in-stm32cubeide
2021-04-02 3:28 PM
I ended up creating a new dummy project in CubeMX using the target MCU, STM32G431C8Ux.
I then put the resulting *.LD file in my target project folder in place of the old LD file.
Next, I opened the project and under Project->Properties->C/C++ Build->Settings->Tool Settings->MCU GCC Linker I changed the linker script to the new name: STM32G431C8UX_FLASH.ld
Then I rebuilt and got the desired results.
Brian