2022-02-03 11:23 PM
Hi, i have a custom board with STM32H750 with qspi flash and want to debug with j-link debugger. Before i used it with st-link and my custom flashloader while debugging. Now i want to write open loader for my project but i didn't see any settings how to add this loader to STM32CubeIDE.
For example, when i select st-link in debug configurations i can select and load my custom external loader under misc section.
Solved! Go to Solution.
2023-05-23 6:50 AM
No, when you entered debug mode in cubeide, it will program internal and external flash automatically. You don't need to program external flash with cubeprogrammer.
You will see in cubeide console when you are entering debug mode like that:
------------------------------------------------------------------------------------------------------
Erasing memory corresponding to segment 0: // Internal flash programming
Erasing memory corresponding to segment 1: // Internal flash programming
Erasing external memory sectors [0 56] // External flash programming
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:16.150
2023-05-23 7:27 AM
Thank you very much for the input. I will give the ST-LINK external loader a try.