2021-04-29 04:27 AM
Hi, I am seung-woo.
I bought two STEVAL-DPSLLCK1. How can I get a firmware for STEVAL-DPSLLCK1?
In, STSW-DPSLLCK1 - STM32F334 full bridge LLC firmware package for STEVAL-DPSLLCK1 - STMicroelectronics
I was download "en.stsw-dpsllck1.zip". However, in the file, only one 55kb binary file.
How can I get a full project file?
Regards.
2021-05-28 09:22 AM
I'm looking for the same files.
I'd appreciate any help from ST side.
Thank you!
2021-06-17 08:10 PM
So u get the IAR/EWARM project file?
2021-09-21 01:02 PM
Same problem. Couldnt find the files... Any help is very appreciated.
2022-09-16 01:14 AM
Hello ST,
Maybe you have forgotten to upload the files.
We are looking for the source code. It says in the manual like this:
There seem to be no restrictions stated in the brief.
2022-11-28 11:42 PM
I am also looking for the same. Appreciate any help from STM.
@AShei.1 @AMao.1 @[AVilk.1] Any of you got access to source code?
2022-12-05 05:48 PM
You can download the firmware at https://eds.st.com/llc/
2022-12-19 02:53 AM
2023-01-13 03:27 PM
Archive has check sum errors and cannot be extracted. Same for archive from eds.st.com/llc
Do you have a working on?