cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I am using STEVAL-STLKT01V1 and NUCLEO-F303RE and need to run AudioLoop from ac6 System Workbench for STM32 Project. I imported the code and run it but I am getting this error: No source available for "main() at 0x8004304" What can I do?

ARami.2
Associate II

This is what I have:

0693W00000FATePQAX.jpg 

The system works fine with DataLog. The problem is when I run AudioLoop. What I see is that the COM port is enabled with DataLog and then I run Putty and see the results in real time. However, the COM port is never enabled when I run AudioLoop. Is the AudioLoop code incomplete? Should I configure something in IDE Workspace 1.7.0? Is there any place where I can find a solution or at least the detail instructions fixing this issue to run AudioLoop?

0 REPLIES 0