2020-04-28 08:31 AM
Hello
I'm trying a project with a STM32L051R8T6 microcontroller and STM32CubeIDE, I already finished my code and tested in a board, everything worked fine . I've not modified the code, anf now I can't enter in Debbug mode.
I tested the ST-Link with other of my projects and it is working fine, the problem is with this new development that I'm trying. I have three boards prototype and the error still occurring with all of them.
Please check the attached files with error message.
Can you help me to solve?
2020-04-28 08:37 AM
This is the output in Console:
--------------------------------------------------------------------------------------------
STMicroelectronics ST-LINK GDB server. Version 5.4.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Users\salva\STM32CubeIDE\workspace_1.2.0\DMX\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
InitWhile : Enabled
Target connection mode: Under reset
Hardware watchpoint supported by the target
COM frequency = 4000 kHz
ST-LINK Firmware version : V2J35S7
Device ID: 0x417
PC: 0x8001220
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.21 V
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x0000000B
NVIC_CFGFSR_REG = 0x00000000
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x00000008
NVIC_CFGFSR_REG = 0x00000000
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.3.0
-------------------------------------------------------------------
Log output file: C:\Users\salva\AppData\Local\Temp\STM32CubeProgrammer_a06320.log
ST-LINK SN : 56FF71067878545233240667
ST-LINK FW : V2J35S7
Voltage : 3.21V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x417
Device name : STM32L05x/L06x/L010
Flash size : 64 KBytes
Device type : MCU
Device CPU : Cortex-M0+
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a06320.srec
File : ST-LINK_GDB_server_a06320.srec
Size : 16084 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 125]
Download in Progress:
�������������������������������������������������� 0%
�������������� 28%�������������� 57%�������������� 85%�������� 100%
Error: failed to download Segment[0]
Error: failed to download the File
Time elapsed during download operation: 00:01:02.659
Verifying ...
Read progress:
�������������������������������������������������� 50%
������ 12%��� 19%��� 25%��� 31%���� 38%��� 44%��� 50%��� 57%��� 63%���� 70%��� 76%��� 82%��� 89%��� 95%��� 100%
Error: Data mismatch found at address 0x08003A6C (byte = 0x00 instead of 0xFF)
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.2.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.1.0.201910081157\tools\bin\STM32_Programmer_CLI.exe
------ Switching context -----
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
--------------------------------------------------------------------------------------------