Hello,
Problem with new firmware version FW_F7 V1.16.1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-25 5:27 AM
When i open my .ioc file a popup windows appears with
"this project was setup using STM32Cube firmware version FW_F7 V1.16.0 then new STM32Cube V6.2.1 works best with ...."
I've tried the two options "continue" and "update" after that i have the following errors when i build my project after the code generation
c:\st\stm32cubeide_1.4.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/system_stm32f7xx.o:C:/V2_TEST/Debug/../Drivers/CMSIS/Device/ST/STM32F7xx/Include/system_stm32f7xx.h:74: multiple definition of `SystemCoreClock'; Core/Src/system_stm32f7xx.o:C:/V2_TEST/Debug/../Drivers/CMSIS/Device/ST/STM32F7xx/Include/system_stm32f7xx.h:74: first defined here
c:\st\stm32cubeide_1.4.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/system_stm32f7xx.o:(.rodata.AHBPrescTable+0x0): multiple definition of `AHBPrescTable'; Core/Src/system_stm32f7xx.o:(.rodata.AHBPrescTable+0x0): first defined here
c:\st\stm32cubeide_1.4.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/system_stm32f7xx.o:(.rodata.APBPrescTable+0x0): multiple definition of `APBPrescTable'; Core/Src/system_stm32f7xx.o:(.rodata.APBPrescTable+0x0): first defined here
c:\st\stm32cubeide_1.4.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/system_stm32f7xx.o: in function `SystemInit':
C:/V2_TEST/Debug/../Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/system_stm32f7xx.c:135: multiple definition of `SystemInit'; Core/Src/system_stm32f7xx.o:C:/V2_TEST/Debug/../Core/Src/system_stm32f7xx.c:135: first defined here
c:\st\stm32cubeide_1.4.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/system_stm32f7xx.o: in function `SystemCoreClockUpdate':
C:/V2_TEST/Debug/../Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/system_stm32f7xx.c:186: multiple definition of `SystemCoreClockUpdate'; Core/Src/system_stm32f7xx.o:C:/V2_TEST/Debug/../Core/Src/system_stm32f7xx.c:186: first defined here
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:137: Labopur.elf] Error 1
Any clue or workaround ? It's very annoying because now it is impossible to modify my hardware definition ..
Regards
Stéphane
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-25 6:34 AM
> C:/V2_TEST/Debug/../Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/system_stm32f7xx.c:186: multiple definition of `SystemCoreClockUpdate';
The "templates" folder should not be part of the source folders you compile. Delete it from there, or exclude that directory from the build.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-25 6:34 AM
> C:/V2_TEST/Debug/../Drivers/CMSIS/Device/ST/STM32F7xx/Source/Templates/system_stm32f7xx.c:186: multiple definition of `SystemCoreClockUpdate';
The "templates" folder should not be part of the source folders you compile. Delete it from there, or exclude that directory from the build.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-25 9:16 AM
Problem solved
Thank you