cancel
Showing results for 
Search instead for 
Did you mean: 

Hello. How can I measure the length of an indefinite length "uint8_t"? I used sizeof() but it didn't measure correctly

ZKURT.1
Senior

0693W00000NpgVjQAJ.png

12 REPLIES 12
ZKURT.1
Senior

#define ElemanSayisi 1000

uint8_t buffer[ElemanSayisi] =

{ 6, 4, 0, 7, 7, 1, 7, 6, 5, 3, 1, 3, 3, 0, 6, 2, 4, 9, 1, 9, 2, 2, 5,

1, 1, 9, 6, 7, 4, 4, 2, 6, 5, 7, 4, 7, 4, 2, 3, 5, 5, 3, 4, 9,

1, 9, 4, 9, 3, 4, 9, 6, 9, 8, 3, 5, 2, 0, 3, 1, 2, 7, 7, 4, 5,

0, 6, 3, 2, 6, 2, 3, 9, 5, 7, 8, 3, 1, 8, 0, 1, 6, 9, 8, 4, 8,

0, 1, 8, 6, 9, 4, 7, 8, 8, 5, 1, 8, 4, 3, 8, 5, 8, 6, 1, 5, 6,

0, 7, 8, 9, 1, 1, 2, 9, 4, 9, 4, 9, 5, 4, 5, 9, 5, 0, 1, 7, 3,

7, 9, 5, 8, 3, 3, 1, 9, 5, 2, 8, 5, 3, 2, 0, 8, 8, 0, 5, 5, 1,

1, 1, 2, 5, 4, 0, 6, 9, 8, 7, 4, 7, 1, 5, 8, 5, 2, 3, 8, 6, 3,

0, 5, 0, 7, 1, 5, 6, 9, 3, 2, 9, 0, 9, 6, 3, 2, 9, 5, 2, 2, 7,

4, 4, 3, 0, 4, 3, 5, 5, 7, 6, 6, 8, 9, 6, 6, 4, 8, 9, 5, 0, 4,

4, 5, 2, 4, 4, 5, 2, 3, 1, 6, 1, 7, 3, 1, 8, 5, 6, 4, 0, 3, 0,

9, 8, 7, 1, 1, 1, 2, 1, 7, 2, 2, 3, 8, 3, 1, 1, 3, 6, 2, 2, 2,

9, 8, 9, 3, 4, 2, 3, 3, 8, 0, 3, 0, 8, 1, 3, 5, 3, 3, 6, 2, 7,

6, 6, 1, 4, 2, 8, 2, 8, 0, 6, 4, 4, 4, 4, 8, 6, 6, 4, 5, 2, 3,

8, 7, 4, 9, 3, 0, 3, 5, 8, 9, 0, 7, 2, 9, 6, 2, 9, 0, 4, 9, 1,

5, 6, 0, 4, 4, 0, 7, 7, 2, 3, 9, 0, 7, 1, 3, 8, 1, 0, 5, 1, 5,

8, 5, 9, 3, 0, 7, 9, 6, 0, 8, 6, 6, 7, 0, 1, 7, 2, 4, 2, 7, 1,

2, 1, 8, 8, 3, 9, 9, 8, 7, 9, 7, 9, 0, 8, 7, 9, 2, 2, 7, 4, 9,

2, 1, 9, 0, 1, 6, 9, 9, 7, 2, 0, 8, 8, 8, 0, 9, 3, 7, 7, 6, 6,

5, 7, 2, 7, 3, 3, 3, 0, 0, 1, 0, 5, 3, 3, 6, 7, 8, 8, 1, 2, 2,

0, 2, 3, 5, 4, 2, 1, 8, 0, 9, 7, 5, 1, 2, 5, 4, 5, 4, 0, 5, 9,

4, 7, 5, 2, 2, 4, 3, 5, 2, 5, 8, 4, 9, 0, 7, 7, 1, 1, 6, 7, 0,

5, 5, 6, 0, 1, 3, 6, 0, 4, 8, 3, 9, 5, 8, 6, 4, 4, 6, 7, 0, 6,

3, 2, 4, 4, 1, 5, 7, 2, 2, 1, 5, 5, 3, 9, 7, 5, 3, 6, 9, 7, 8,

1, 7, 9, 7, 7, 8, 4, 6, 1, 7, 4, 0, 6, 4, 9, 5, 5, 1, 4, 9, 2,

9, 0, 8, 6, 2, 5, 6, 9, 3, 2, 1, 9, 7, 8, 4, 6, 8, 6, 2, 2, 4,

8, 2, 8, 3, 9, 7, 2, 2, 4, 1, 3, 7, 5, 6, 5, 7, 0, 5, 6, 0, 5,

7, 4, 9, 0, 2, 6, 1, 4, 0, 7, 9, 7, 2, 9, 6, 8, 6, 5, 2, 4, 1,

4, 5, 3, 5, 1, 0, 0, 4, 7, 4, 8, 2, 1, 6, 6, 3, 7, 0, 4, 8, 4,

4, 0, 3, 1, 3, 9, 8, 9, 0, 0, 0, 8, 8, 9, 5, 2, 4, 3, 4, 5, 0,

6, 5, 8, 5, 4, 1, 2, 2, 7, 5, 8, 8, 6, 6, 6, 8, 8, 1, 1, 6, 4,

2, 7, 1, 7, 1, 4, 7, 9, 9, 2, 4, 4, 4, 2, 9, 2, 8, 2, 3, 0, 8,

6, 3, 4, 6, 5, 6, 7, 4, 8, 1, 3, 9, 1, 9, 1, 2, 3, 1, 6, 2, 8,

2, 4, 5, 8, 6, 1, 7, 8, 6, 6, 4, 5, 8, 3, 5, 9, 1, 2, 4, 5, 6,

6, 5, 2, 9, 4, 7, 6, 5, 4, 5, 6, 8, 2, 8, 4, 8, 9, 1, 2, 8, 8,

3, 1, 4, 2, 6, 0, 7, 6, 9, 0, 0, 4, 2, 2, 4, 2, 1, 9, 0, 2, 2,

6, 7, 1, 0, 5, 5, 6, 2, 6, 3, 2, 1, 1, 1, 1, 1, 0, 9, 3, 7, 0,

5, 4, 4, 2, 1, 7, 5, 0, 6, 9, 4, 1, 6, 5, 8, 9, 6, 0, 4, 0, 8,

0, 7, 1, 9, 8, 4, 0, 3, 8, 5, 0, 9, 6, 2, 4, 5, 5, 4, 4, 4, 3,

6, 2, 9, 8, 1, 2, 3, 0, 9, 8, 7, 8, 7, 9, 9, 2, 7, 2, 4, 4, 2,

8, 4, 9, 0, 9, 1, 8, 8, 8, 4, 5, 8, 0, 1, 5, 6, 1, 6, 6, 0, 9,

7, 9, 1, 9, 1, 3, 3, 8, 7, 5, 4, 9, 9, 2, 0, 0, 5, 2, 4, 0, 6,

3, 6, 8, 9, 9, 1, 2, 5, 6, 0, 7, 1, 7, 6, 0, 6, 0, 5, 8, 8, 6,

1, 1, 6, 4, 6, 7, 1, 0, 9, 4, 0, 5, 0, 7, 7, 5, 4, 1, 0, 0, 2,

2, 5, 6, 9, 8, 3, 1, 5, 5, 2, 0, 0, 0, 5, 5, 9, 3, 5, 7, 2, 9,

7, 2, 5, 7, 1, 6, 3, 6, 2, 6, 9, 5, 6, 1, 8, 8, 2, 6, 7, 0, 4,

2, 8, 2, 5, 2, 4, 8, 3, 6, 0, 0, 8, 2, 3, 2, 5, 7, 5, 3, 0, 4,

2, 0, 7, 5, 2, 9, 6, 3, 4, 5, 0, };

uint8_t *arr = (uint8_t*) &buffer; 

int ***(uint8_t *arr, int x) {

}

It's done this way.

0693W000008xsqBQAQ.png 

Note that it's conventional to use ALL UPPERCASE for #defined names - to distinguish them from variables (or functions).

uint8_t *arr = (uint8_t*) &buffer;

Your pointer arr is redundant here - why not just use buffer direct?

If your issue is now resolved, please mark the solution: 

0693W000008y9fZQAQ.png

then you cannot use buffers that are not 1000 long in that foo() function.

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero