2020-09-04 5:40 AM
Hi everyone.
I want to use SystemView to log data from stm32f429I-disc1. I generated code by CubeMX 6.0.1 to run FreeRTOS on my boad. FreeRTOS Interface is CMSISv2, and it has two simple tasks which both of them run os_delay(1). I went step by step according to a tutorial on youtube and added necessary changes to my project.
The problem is when microcontroller wants to execute os_delay from second task, it goes to HardFault_Handler. I increased stack size of each task, even increased Minimum Heap Size and Stack Size but nothing is changed.
target board: STM32F429I-DISC1
CubeMX version: 6.0.1
CubeIDE version: 1.4.2
CMSIS package version: 5.6
SystemView source version: 312
tutorial which I followed:
https://www.youtube.com/watch?v=1YiWFV_YbsM&list=PLvy7FusYCoHYvHstE1fGjehMLhaJBbiKk
.ioc file is attached.
TNX
Solved! Go to Solution.
2020-09-04 6:02 AM
Suddenly I disabled USB_OTG_HS and it woks:|
2020-09-04 6:02 AM
Suddenly I disabled USB_OTG_HS and it woks:|