cancel
Showing results for 
Search instead for 
Did you mean: 

Getting trouble with USART data transfer with STM32429I-EVAL1

Unlimit
Associate II

Hello,

I'm trying to do USART data transferring with STM32429I-EVAL1 board.

I used example code on CubeIDE and did nothing to the code.

I connected ST-Link/V2 and USART RS-232 cable to my PC.

 

Then, I got lots of broken letters appears on terminal. (few of them are correct, but almost over 90% of letters are broken)

 

I checked baud rate, stop bits, parity bits, control flow etc. are same with the code.

I don't know how to solve it. Can anybody help me?

 

7 REPLIES 7
mƎALLEm
ST Employee

Hello,

Could you please indicate  which example you are using?

Check first your RS232 cable. It could be a bad contact.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Andrew Neil
Super User

@Unlimit wrote:

Then, I got lots of broken letters appears on terminal.


When you get "junk" characters on a terminal, that generally means your baudrate is wrong:

https://community.st.com/t5/stm32-mcus-wireless/uart-reception-isssue/m-p/684276/highlight/true#M19562

 


@Unlimit wrote:

I checked baud rate,


How did you check it?

See the above link for how to check for sure...

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I bought RS232 cable a few days ago but how can I check its connect is right?

And I'm using "UART printf" example for STM32429I-EVAL1.

In the example code, baudrate is set as 9600 in default.

I did not edit it and I cannot configure it with .ioc file, so I think it's right.

If not, how can I check the baudrate without configuring?

You could perhaps check with a multi-meter, look at signals with an oscilloscope or a logic analyzer.

This stuff is very hard diagnose remotely with vague and non-specific details.

What cable, wired how? Perhaps link to page for whatever you bought.

RS232, for sure? Your machine has a serial port? Is this a USB to Serial adapter? CMOS or RS232 Levels?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Perhaps send a lot of 'U' characters, and inspect the signal with a scope?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I don't have any multi-meter nor oscilloscope etc.

My board has RS-232 USART port and I plugged it into my PC USB port.

ST-link cable is connected samely.

As I saw the document of the board, I can only see one USART port which I plugged in.