2024-07-11 12:52 AM - edited 2024-07-11 12:53 AM
Following up from my previous post, I am having issues with code generation - it seems to complete, but I don't see anything changed in the code.
Here attached you will find the ioc file. I modified pin names for PB10 to PB12, but after generating the code I don't see any of the name in the project (should be in main.h, but I did a search in the whole project just to be sure).
I am using STM32CubeIDE 1.16.0 on mac Sonoma 14.2.1 with M1 chip.
Solved! Go to Solution.
2025-01-09 01:32 PM - edited 2025-01-09 01:55 PM
Hey all. I have this same issue. I have the following installed:
STM32CubeMX - 6.13.0
STM32CubeProgrammer - 2.18.0
STM32CubeIDE - 1.17.0
The device I'm trying to generate for is the STM32H747XI. I have tried clearing the myST account info and entering it again (from CubeMX and from CubeIDE). Regardless of which app I try to generate code from, I never get more than a skeleton (e.g. none of the custom User Labels for PINs show as #defines, and there's no initialization code generated). The Check Connection button always returns without a displayed error, there's no Proxy server in use.
Any ideas?
Thanks - C-Coder
EDIT - Looks like the problem was that the Pin Context Assignment value was not set. Set them to the appropriate core causes the code to be generated.