Solved
Missing definition of type "SPI_HandleTypeDef"
- 4 replies
- 3037 views
I have configured a STM32 project in the ioc interface to use SPI2 - I can see it having the green check mark in the ioc interface. However when I generate code I don't see any spi driver header, and when compiling I get a:
error: unknown type name 'SPI_HandleTypeDef'; did you mean 'TIM_HandleTypeDef'?I am using the STM32CubeIDE version 1.16.0 on mac.