cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to execute MI command

I am trying to debug my hardware for the first time. I was working in TrueStudio 9.3.0 as I had started this project in it before STM32CubeIDE came out. When I started to try to debug my program to day I got an error. OK, maybe I should try STM32CubeIDE instead. Loaded this up and got the project migrated with no problem. But when I go into the debugger it generates the same error and exits. I am not sure where to start to track this down. The console shows this:

STMicroelectronics ST-LINK GDB server. Version 5.2.3

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

Waiting for debugger connection...

Debugger connected

Debugger connection lost.

Shutting down...

The detailed error message gives me this:

Error in final launch sequence:

Failed to execute MI command:

target remote localhost:61234

Error message from debugger back end:

Remote communication error. Target disconnected.: Success.

Failed to execute MI command:

target remote localhost:61234

Error message from debugger back end:

Remote communication error. Target disconnected.: Success.

Remote communication error. Target disconnected.: Success.

I am using an ST-LINK\V2. I can download the program just fine using STM32CubeProg so I know the ST-LINK and the interface is working correctly. Where do I go next to figure this out? Thanks.

20 REPLIES 20
Ricarry
Associate

I solved that error by activating serial wire in pinout and configurations > sys > debug: serial wire