cancel
Showing results for 
Search instead for 
Did you mean: 

Facing the issue while integrating CubeAI and CubeIDE

jainamaster14
Associate

I am trying to make a voice controller light with the help of STM32F411RE. I have trained a model with the help of google colab and imported it in both the format that is .h5 and .tflite but initially it was showing that the space is full and then after the compression of model this issue was resolved. The issue that I m facing now is that nothing is printing on the console and without the usage of CubeAI my code is running smoothly but if i try to deploy my model on it then nothing is showing so what to do? 

I have attached the code below please refer to it

0 REPLIES 0