cancel
Showing results for 
Search instead for 
Did you mean: 

Facing issue while creating external flash loader

Nagarajan
Associate III

I am using NUCLEO-H563ZI evaluation board and i want to create external flash loader for IS25LP128 QSPI flash memory. I used external loader files from GIT HUB and .stldr file in STCUBE programmer external loader folder location. when i try to read from 0x90000000 location, i am getting read failure error. I used the below path to create external loader for IS25LP128 QSPI flash memory,

stm32-external-loader/Loader_Files/other devices at contrib · STMicroelectronics/stm32-external-loader · GitHub

Could you please help me to solve the below issue?

 

Nagarajan_2-1711548543593.png

 

 

54 REPLIES 54

Quick rework posted   https://github.com/cturvey/stm32extldr/blob/main/h7_is25lp128/CLIVEONE-IS25LP128_STM32H72X-PA3-PC11-PC9-PC10-PE2-PA6.stldr

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks a lot!

Sadly, no visible change: When the flash device is in QPI mode, the external loader doesn't work, it works when QPI is off.

Where can I find the souce of it? Maybe, I can look at it too, either to learn, or to improve, with my limited competency, but quite good knowledge of this memory chip and a test setup.

hello!

did you succes in making the external loader?

i have tried your suggestion but mine don't work

i have a working driver for MX25L512 but  i 'm not able to have a working external loader

if you succed can you share your project?

 

thank yoy 

 

Andrea

How to enable QE bit without sending 35h? I had tried enabling QE bit by sending Write status register and data 40h along with it.

Yes, you should be able read/write the register and set bits.

Can you read the JEDEC ID ?

Does the device work in 1-bit and 2-bit modes?

In some QSPI memories the QE bit relates to the pin mode/availability, not the operational mode for the command.

Perhaps present your case/situation more completely? 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..