2019-11-19 08:26 AM
Goodevening,
I'm new on this community and i I want to apologize in advance if I make some mistake. My problem is: when i create new STM32 project i get this error "Code generation could not be done because the necessary firmware package is missing. Not able to complete STM32Cube project creation". I try the different solution proposed in the discussion but noone works, I'm really desperate because I need it for university. I will be happy to give you other details if needed.
thank you.
2019-11-19 01:54 PM
Have you access to external world (i.e. allowing some donwload from www ?). Good way to double check is to have a try to access to Eclipse market place Help > MarketPlace. If not Please have a look to Windows > Preferences Network Settings.
STM32Cube project generation is requiring some local FW package. If not available will be downloaded for you ... but external world access is must have.
2019-11-20 12:06 AM
hi,
i've just try your solution, the access to marketplace works fine, but the error still appair. I've try to install the ide on diffrent notebook, and when i create a new project it has been completed with no errors and i don't know why. Is it possible that this error is referenced to an architecture? BC the installation failed on AMD architecture but no in intel.
2019-11-20 12:24 PM
Which target are you using ? If F4 serie one sounds some trouble may exist currently : https://community.st.com/s/question/0D50X0000BeZi12SQC/code-generation-could-not-be-done-firmware-package-v1241-can-not-be-unzipped
2019-12-03 01:36 AM
I have the same problem with all Fx series. The package was downloaded to the rep and unpacked successfully. I tried to download all necessary files manually. I checked Firmware Updater - the connection is ok. I changed firmware repository, project name, workbench location. I tried to reinstall on 3 computers (Win10 Intel i3-8100 and i5) But I still receive: "Code generation could not be done..." Is there a real working solution?