2023-07-21 2:10 AM
Hello @RMcCa
I am working on the same area where i want to write variable in shared memory of SRAM4 via M4 and to read from M7.
I have gone through your post Best/easiest way to share data between cores in ST... - STMicroelectronics Community
Could you please let me know how to do sharing and writing reading variable in STM32
Thanks in advance
Solved! Go to Solution.
2023-07-26 5:51 AM - edited 2023-07-26 5:52 AM
Hello @Nsg1987,
Thank you for highlighting a frequent topic/question. Here is an example developed by our colleague in which you can test Inter-CPU asynchronous communication. However, I guess we cannot judge if this is the best or easiest way to share data between two cores.
Hope this helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-23 8:05 AM
Generating a duplicate topics for the same issue is spamming. Why are you spamming?
An you have already received all the details in your previous topic:
2023-07-26 5:51 AM - edited 2023-07-26 5:52 AM
Hello @Nsg1987,
Thank you for highlighting a frequent topic/question. Here is an example developed by our colleague in which you can test Inter-CPU asynchronous communication. However, I guess we cannot judge if this is the best or easiest way to share data between two cores.
Hope this helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-26 3:28 PM
That link was in the topic, which he said he did read, and it was also recently already given to him specifically and the reaction was: "Could you share any other way..." Beginners cannot do everything - one has to learn things.