2024-11-16 07:13 AM
My issue is quite simple, I want larger fonts.
I would ask you for "Even Larger", and then for "Huge" when 8K screens are more common (or when my eyesight gets worse), but I suggest we stop playing this silly game.
Instead, I propose that we should specify scale as a floating-point number, just as god intended.
Thank you
Solved! Go to Solution.
2024-11-16 07:44 AM - edited 2024-11-17 11:44 PM
Hello @bean and welcome to the ST Community.
I've escalated your request to the concerned team to review the possibility to implement it on the future (under internal ticket number 196437).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-16 07:44 AM - edited 2024-11-17 11:44 PM
Hello @bean and welcome to the ST Community.
I've escalated your request to the concerned team to review the possibility to implement it on the future (under internal ticket number 196437).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-16 08:17 AM
@STTwo-32 thank you, that will be much appreciated.
This minor change will greatly affect usability for people in my predicament, which I predict is perhaps not large but also not an insignificant group.
Also, if there are existing workarounds to achieve this control over the UI scale or even just the font size, some direction will also be appreciated.