2025-01-14 8:23 AM
Hi All,
I am working on a project in CubeIDE workspace 1.17.0 and am having issues with my custom application source files not being indexed properly. My new files are being included in the build properly and the code from them is running, but the files in the editor remain purely "gray" text and lack the ability to jump to function defs/decs through them. I have tried restarting the IDE as well as using the Project->C/C++ Index options in the menu. Thanks in advance!
2025-01-15 1:25 AM
Hello @dlewis
A few things to check:
THX
Ghofrane