2021-04-15 04:29 AM
This is less of a question and more of a statement for your information. I was not able to install the v1.6.0 update and have just been ignoring the notifications for a while, so when I saw that v1.6.1 was available I thought I'd try that but it still fails. I've attached a screenshot of the error output. There were many more rows but all to the same effect.
Also I am on macOS Big Sur 11.0.1 and my current version of CubeIDE is v1.5.1.
Thanks!
Matt
Solved! Go to Solution.
2021-04-28 07:26 AM
Indeed, to access deeper into an .app you either have to do it thanks to "Right click > Show Package Contents" or using a Terminal.
Not fully compliant with Big Sur means that you might face some troubles. Anyway we don't expect more issues with 1.6.1 than you could already have with 1.5.1. Both versions are based on the same Eclipse platform.
2021-04-15 05:00 AM
Hi MKeff.1,
Did you tried to apply the workaround, aiming to cleanup the updater cache, already shared on the Forum?
Regardless the update issue, be aware that STM32CubeIDE is not fully compliant with Big Sur.
HTH
2021-04-28 07:01 AM
Hi Julien, no I didn't try that already. I did look before asking but I didn't see the post you refer to.
I closed CubeIDE and looked for STM32CubeIDE.app which I found in Applications (makes sense!). I cannot open it though to navigate further to STM32CubeIDE.app/Contents, if I open it it just starts the app. So I don't understand your instruction number 2.
It sounds like I should just stick with my current version though based on what you said! So I will stick with v1.5.1 for now
Thanks!
2021-04-28 07:26 AM
Indeed, to access deeper into an .app you either have to do it thanks to "Right click > Show Package Contents" or using a Terminal.
Not fully compliant with Big Sur means that you might face some troubles. Anyway we don't expect more issues with 1.6.1 than you could already have with 1.5.1. Both versions are based on the same Eclipse platform.