cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE and External Flash

Peaga
Senior

Hello there!

I know most ST uprocessor can work really well extending the internal flash to a Quad Flash. In Keil, I can easily create a FLM file (flash algorithm) and start debugging the project with only one click, even when part of the code is in the internal flash. But in TrueStudio, I can't make it work that way and most ST examples puts a "boot" in internal and tha "app" in external.

Is CubeIDE a little better? Or do you know another way closer to Keil?

Thanks a lot!

1 REPLY 1

@Andreas Bolsch​  has some external flash support for OpenOCD

ST support via External Loaders in ST-LINK Utilities and STM32 Cube Programmer

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..