cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE 1.6.0 - Code generation freezes on project done on previous version.

slawek
Associate III

After installation of CubeIDE 1.6.0 Code generation freezes and never unlocks.

Project was done on previous version of CubeIDE with firmware version 1.24.1. When I try to migrate it doesn't change anything. But if I use the same IOC for generation of new project it doesn't hangup.

9 REPLIES 9
Cartu38 OpenDev
Lead II

could you share <workspace>/.metadata/.ide.log file and possibly .ioc file ?

slawek
Associate III

Regrading IOC I would need to obfuscate it a little bit. log looks like this:

It looks like it hangs up on access to: http://sw-center.st.com:80

2021-03-26 15:20:20,386 [INFO] ApiDbMcu:458 - Load IP Config File for PDM2PCM

2021-03-26 15:20:20,417 [WARN] FreeRTOS:989 - Null or empty value: should not occur! (nothing added to the table)

2021-03-26 15:20:20,502 [INFO] LogOutputStream:76 - [STDOUT_REDIRECT] toolchainItems.length=====1

2021-03-26 15:20:20,602 [INFO] RtosManager:597 - Active RTOS found at IOC load: FREERTOS [Cortex-M4NS]

2021-03-26 15:20:20,602 [INFO] OpenFileManager:323 - Restore cursor

2021-03-26 15:20:21,804 [ERROR] LogOutputStream:74 - [STDERR_REDIRECT] Managed Build system manifest file error: Could not load icon "icons/chip.png".

2021-03-26 15:20:21,804 [ERROR] LogOutputStream:74 - [STDERR_REDIRECT] Managed Build system manifest file error: Could not load icon "icons/chip.png".

2021-03-26 15:20:21,804 [ERROR] LogOutputStream:74 - [STDERR_REDIRECT] Managed Build system manifest file error: Could not load icon "icons/chip.png".

2021-03-26 15:20:44,093 [INFO] RetryExec:97 - I/O exception (org.apache.http.NoHttpResponseException) caught when processing request to {}->http://sw-center.st.com:80: The target server failed to respond

2021-03-26 15:20:44,093 [INFO] RetryExec:113 - Retrying request to {}->http://sw-center.st.com:80

Initiating a new session is Help > Check for Updates able to complete ?

If not fix your remote access. Doing migration process some db download is required. If not able may explain ...

slawek
Associate III

"Help > Check for Updates" is working correctly.

Are you able to get following green check ?

0693W000008y2guQAA.jpg

slawek
Associate III

Yes

slawek
Associate III

now log during generation hangs in different place:

2021-03-26 17:15:19,651 [INFO] ApiDbMcu:458 - Load IP Config File for FREERTOS

2021-03-26 17:15:19,713 [INFO] ApiDbMcu:458 - Load IP Config File for LWIP

2021-03-26 17:15:19,713 [WARN] BspModel:441 - BSP dependency skipped because of component: name='LAN8742', api='BSP_COMPONENT_DRIVER'

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,744 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,751 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,766 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,767 [INFO] IPUIPlugin:64 - create IPUIPlugin

2021-03-26 17:15:19,768 [INFO] ApiDbMcu:458 - Load IP Config File for PDM2PCM

2021-03-26 17:15:19,783 [WARN] FreeRTOS:989 - Null or empty value: should not occur! (nothing added to the table)

2021-03-26 17:15:19,866 [INFO] LogOutputStream:76 - [STDOUT_REDIRECT] toolchainItems.length=====1

2021-03-26 17:15:19,967 [INFO] RtosManager:597 - Active RTOS found at IOC load: FREERTOS [Cortex-M4NS]

2021-03-26 17:15:19,967 [INFO] OpenFileManager:323 - Restore cursor

slawek
Associate III

It looks, that with the newest update (Version: 1.6.1 Build: 9958_20210326_1446 (UTC)) of CubeIDE problem disappeared.

Thanks for sharing. Thinking on my side local issue. Updating your IDE has just helped to perform some local state refresh.

Hopefully working now for you !