cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE 1.21 causes 100% processor usage.

HHarj.1
Senior

CubeIDE 1.21 causes 100% processor usage and slows down the computer. Even worse is closing the program doesn't free up the resources, the usage still stays 100%. The task manager shows that cubeide.exe closes, but still the issue stays. I'm running windows 7 pro x64.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
dbgarasiya
Senior II

just remove and againg install,

otherwise problem may be in your pc

dbgarasiya
Senior II

mostly it depends on ram

My computer has 16GB of ram, task manager shows about 10GB in use, so that shouldn't be an issue. I have also a laptop where it runs normally (windows 10). BTW, Cubeide 1.1 run normally. Problems started when started using 1.2.

Ozone
Principal III

Other Eclipse-nased tools use to run for a couple of seconds after closing as well, so this is nothing special.

After a minute at latest, it should be gone.

Check the ressource usage at runtime, before and during operation. Including HD throughput.

And I would try with the network cable pulled out.

dbgarasiya
Senior II

just submit a ticket to silabs