cancel
Showing results for 
Search instead for 
Did you mean: 

CUBE IDE No source available for "<signal handler called>() at 0xfffffffe" Errors

ark2
Associate III
 

I was making a project with CUBE IDE and compiling it on the board, and I got this error while compiling the project I was doing on the new board.

No source is available for "Call Signal Handler"() in 0xfffffffe.

I'm sure they're using the same CPU

I can't compile it because it's STM32 ST-LINK

I don't think there will be any problems with the code or MX settings because if I modify the code on the existing board, the project will also change well.



Even if I create a new project and add the above code, I get the same error, so I can't compile it

I want to solve this phenomenon, how do I solve it?

 

 

int main(void)
{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MPU Configuration--------------------------------------------------------*/
  MPU_Config();

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  /* USER CODE BEGIN 2 */

  HAL_GPIO_WritePin(GPIOK, GPIO_PIN_2, GPIO_PIN_SET);

  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

 

 

The same error occurs in the above simple code.

How can I fix this problem?

 

stm32 : STM32H743XIH6

==========================================

Error image

01.JPG

=========================================
Current state

00.JPG

 

01.JPG

 

02.JPG

 

03.JPG

 

 

 

1 REPLY 1
Andrew Neil
Evangelist III

0xfffffffe is a "magic" address in the ARM Cortex-M architecture which indicates a core lockup; eg, a double Hardfault:

https://forum.microchip.com/s/topic/a5C3l000000UjLaEAK/t187425#:~:text=The%20magic%20PC%20value%20of%200xfffffffe%20indicates%20core%20lock%2Dup.%20This%20generally%20happens%20when%20the%20CPU%20double%2Dhardfaults.%20For%20example%2C%20a%20CPU%20hardfault%20occurs%2C%20and%20another%20fault%20occu....

https://developer.arm.com/documentation/ddi0403/d/System-Level-Architecture/System-Level-Programmers--Model/ARMv7-M-exception-model/Unrecoverable-exception-cases?lang=en

 


@ark2 wrote:

I was making a project with CUBE IDE and compiling it on the board, and I got this error while compiling the project


Note that this is not an error that you'd get while compiling: this is a runtime error - it means your code is crashing while it's running on your board.

 


@ark2 wrote:
I can't compile it because it's STM32 ST-LINK

That makes no sense. What do you mean by that?

 


@ark2 wrote:
 

Even if I create a new project and add the above code, I get the same error, so I can't compile it


Again, the message has nothing to do with compiling.

Does the code build cleanly - ie, with no errors and no warnings?