cancel
Showing results for 
Search instead for 
Did you mean: 

Cube gives warning to enable non-existent setting on U575 project

Eqqman
Associate III

When compiling code for the U575 from the IOC file a warning pops up that SMPS must be enabled.  However, we cannot find this setting under the PWR tab nor via the A-Z listing of properties.  What must be done to clear this warning?

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @marrob @Eqqman 

Sorry for my late replay. To enable SMPS on the STM32U575ZIT6Q using the Pinout & Configuration menu on the .ioc file of your project, you have to go to Power and Thermal -> PWR -> Low Power -> check the Case Power saving mode -> on the Power Saving tab under Configuration, change the Power Regulator from LDO to SMPS. for the Pop-up message, you can ignore it clicking on the yes button of the Message. It is just a warning to have better configurations. You can't disable it but you are not obliged to follow it.

STTwo32_0-1721661889452.png

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Hello @Eqqman 

Can you add more details (which MCU are you using exactly and which CubeMX version).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STM32CubeIDE

 

Version: 1.15.0

Build: 20695_20240315_1429 (UTC)

 

Also happened with the previous version of the software. Chip selected is STM32U575ZITxQ.

marrob
Associate

It is still problem with STM32U575ZIT6Q

 

STM32CubeIDE

Version: 1.16.0

Build: 21983_20240628_1741 (UTC)

 

Is there any solution to switch off this warning popup?

STTwo-32
ST Employee

Hello @marrob @Eqqman 

Sorry for my late replay. To enable SMPS on the STM32U575ZIT6Q using the Pinout & Configuration menu on the .ioc file of your project, you have to go to Power and Thermal -> PWR -> Low Power -> check the Case Power saving mode -> on the Power Saving tab under Configuration, change the Power Regulator from LDO to SMPS. for the Pop-up message, you can ignore it clicking on the yes button of the Message. It is just a warning to have better configurations. You can't disable it but you are not obliged to follow it.

STTwo32_0-1721661889452.png

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.