2020-05-05 12:06 PM
Upon building with STM32CubeIDE I just get
> collect2: error: ld returned 1 exit status
> make: *** [makefile:44: help.elf] Error 1
Calling arm-none-eabi-gcc directly gets me
> arm-none-eabi-gcc: error: nosys.specs: No such file or directory
Any suggestions?
2020-05-05 12:08 PM
Not using CubeIDE, show the command line being feed into the linker
2020-05-05 12:11 PM
arm-none-eabi-gcc -o "help.elf" @"objects.list" -l/home/benton/STM32CubeIDE/workspace_1.1.0/ARNE_CRC_SPI/STM32CubeExpansion_Crypto_V3.1.0/AccHw_Crypto/STM32L4/Middlewares/ST/STM32_Crypto_AccHw/Lib/STM32AccHwCryptoV3.1.0_L4_KEIL_slsm1elfspf.lib -mcpu=cortex-m4 -T"/home/benton/STM32CubeIDE/workspace_1.1.0/help/STM32L4A6ZGTX_FLASH.ld" --specs=nosys.specs -Wl,-Map="help.map" -Wl,--gc-sections -static -L/home/benton/STM32CubeIDE/workspace_1.1.0/ARNE_CRC_SPI/STM32CubeExpansion_Crypto_V3.1.0/AccHw_Crypto/STM32L4/Middlewares/ST/STM32_Crypto_AccHw/Lib --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-groupThat is fed into the compiler. Is that enough? If not, where can I see the parameters that are fed into the linker?
2020-05-05 12:27 PM
In the first case, are there any other output lines before the error line?
In the second case, is this gcc from a package intended for the Cortex-M?
JW
2020-06-09 12:45 PM
Thank you, that was helpful for debugging. It was not. After getting the masked error I followed https://community.st.com/s/question/0D50X0000AAGtwq/how-to-include-crypto-library-in-system-workbench-project which helped me.