cancel
Showing results for 
Search instead for 
Did you mean: 

Code Generation would clear my code in `main.c`!

Fei
Associate

Hi,

When I updating the pin assignment information and doing code generation, I find my code, for example, USER CODE part is clear. Why? Is any setup wrong here?

 

 

 

while (1)

{

/* USER CODE END WHILE */

 

/* USER CODE BEGIN 3 */

}

/* U

 

STM32CubeIDE

Version: 1.16.0

Build: 21983_20240628_1741 (UTC)

 MacOS: 14.2.1

6 REPLIES 6
STTwo-32
ST Employee

Hello @Fei and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Could you please attach you .ioc file and a screenshot of the issue if possible.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

LCE
Principal II

My advice:

As soon as you start coding, create another CubeMX dummy project to copy new stuff from there.

Then you are safe from Cube overwriting stuff - and from unwanted HAL/LL library updates.

Andrew Neil
Super User

Please see the posting tips for how to properly post source code:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

Where are you putting your user code?

 

while (1) { /* USER CODE END WHILE */ /* <<< Any code here is OUTSIDE the 'User' block, <<< so WILL get overwritten by code generation */ /* USER CODE BEGIN 3 */ } /* U

 

 

See also: https://community.st.com/t5/stm32-mcus-products/cubemx-and-cubeide-interaction/m-p/767567/highlight/true#M272020

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
int main(void) { /* USER CODE BEGIN WHILE */ // user code /* USER CODE END WHILE */ // NOT user code. Will be deleted! /* USER CODE BEGIN 3 */ // more user code /* USER CODE END 3 */ }
Kudo posts if you have the same problem and kudo replies if the solution works.
Click "Accept as Solution" if a reply solved your problem. If no solution was posted please answer with your own.

@Fei  - Example of correct placement of user code (see the 2nd code block):

https://community.st.com/t5/stm32cubeide-mcus/how-to-covert-the-code-according-to-stm32cubeide/m-p/720546#M30694

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Fei if you prefer video, see this for correct placement of user code:

https://youtu.be/hyZS2p1tW-g?t=573

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.